System

Enables read/write at runtime for some system settings of the network interfaces.
BrowseName
System
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Network interfaces
NetworkInterfaces
List of the network interfaces
WiFiConfiguration
DateTimeConfiguration

Methods

Refresh
BrowseName
Refresh
Refresh the System object configuration based on the current system settings in System Manager.
Reboot
BrowseName
Reboot
Restart the system. For supported operating systems, verify if the user running the FactoryTalk Optix Application has the authorization to perform the operating system restart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.