Wi-Fi modes
Wi-Fi interface operating mode (disabled/adapter/access point).
- BrowseName
- WiFiModeEnum
Values
Value | DisplayName | Description |
---|---|---|
0 | Disabled | The Wi-Fi interface is disabled. |
1 | Adapter | The Wi-Fi interface is used to connect to an existing wireless network. |
2 | Access point | The Wi-Fi interface is used to create a wireless network. |
Provide Feedback