IUANode.Find(browseName)
Returns an
IUANode
C# object. The returned object corresponds to the first child node found in the node children on which the method is invoked. The returned object name corresponds to the argument.IUANode Find(stringbrowseName);
Arguments
- browseName(string)
- TheBrowseNameof the node to find.
Returns
- IUANode
- A C# object that corresponds to the object found.
Example
The following example shows a returned C# object that corresponds to the first
Speed
node child of the Model
node:
var model = Project.Current.Get("Model"); var speed = model.Find("Speed");
Provide Feedback