Develop a filterable list box

Develop a list box filled with random strings that you can filter by entering text into a filter text box.
Application example
NOTE:
Download a sample project:
ExampleApplication-FilterableListBox.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.