Set FactoryTalk Linx Data Bridge server settings
Set
FactoryTalk Linx Data Bridge
server settings to select a FactoryTalk Directory
scope, enable or disable the FactoryTalk Linx Data Bridge
service, or change when diagnostic messages are logged. For FactoryTalk Linx Data Bridge
to update tags, a FactoryTalk Directory
server scope must be selected and the service must not be inhibited.Provide Feedback