Remove Report

Perform the following steps to remove a report:
  1. On the left navigation menu, click
    Reports
    .
  2. Click a component (Site/Area/Work Center/Work Unit) from the hierarchy list.
  3. In the
    Reports
    tab, select the required report name checkboxes from the
    Reports
    table.
  4. Click
    Remove
    .
  5. In the
    Remove reports
    dialog box, click
    Remove
    .
    Remove Reports
    The “Deleted successfully” message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal