Download Report

Perform the following steps to download a reports:
  1. In the
    Reports
    table, on the required report name, click the [] icon to expand.
  2. On the required report, click the [] icon.
    Download Report
The “
Downloaded successfully
” message is displayed.
NOTE:
The units shown in the reports are taken from the Site-level configurations.
The sample report of daily electricity for work units with email message:
Sample Email Message
Report - First Page
Report - Second Page
Third Page Report
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal