Conventions

The following conventions are followed in this document:
  • Text, labels, and icon names that are in the User Interface are mentioned in bold. For example: Click
    Sign in with SSO
    .
  • The URLs and links are mentioned in blue text. For example: Application Link.
  • The Cross-Reference is given in blue text. For example: Getting Started.
  • The toast messages that are displayed on the User Interface are mentioned in the italic text and the quotation. For example: The “
    Updated successfully
    ” message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal