Output Energize (OTE)
The OTE instruction sets or clears the data bit based on rung condition.
Available Languages
Ladder Diagram

Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten
- Members of a structure operand are overwritten
- Except when specified, structure operands are shared by multiple instructions.
Ladder Diagram
Operand | Data Type | Format | Description |
|---|---|---|---|
Data bit | BOOL | tag | Bit to be modified. There are various operand addressing modes possible for the data bit, see Bit Addressing for examples. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
|---|---|
Prescan | The data bit is cleared to false |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in. The data bit is cleared to false |
Rung-condition-in is true | Set Rung-condition-out to Rung-condition-in. The data bit is set to true. |
Postscan | The data bit is cleared to false. |
Example
Ladder Diagram

When switch is true, the OTE instruction sets Light_01 to true. When switch is false, the OTE instruction clears Light_01 to false.
Provide Feedback