Configuring FactoryTalk Optix to connect to FactoryTalk DataMosaix SaaS

Make sure that you have installed the
FactoryTalk Optix Studio
application on your system. Once you select the source type as
FactoryTalk Optix
in the Source Info section, a link to download the application will appear (Get FactoryTalk Optix). You can also download the
FactoryTalk Optix Studio
from
FactoryTalk Hub
. For more information on installation, refer to Install FactoryTalk Optix Studio.
Perform the following steps to configure
FactoryTalk Optix
to connect to
FactoryTalk DataMosaix SaaS
:
  1. Launch the
    FactoryTalk Optix Studio
    application.
  2. To open a
    FactoryTalk Optix
    project:
    • For existing projects, click any project from the
      Recent projects
      section.
      Open Existing Project
    • For a new project, click
      New
      [+].
  3. Provide the
    Name
    and
    Location
    details.
    New FactoryTalk Optix Project
  4. Click
    Create
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal