Auditing
The audit trail is a chronological, tamper‑resistant log of important actions that happen in did , , and , so that we can:
FactoryTalk DataMosaix SaaS
. It records who
what
when
to which object
- Demonstrate data integrity and regulatory compliance.
- Investigate incidents and suspicious activity.
- Understand configuration and data changes over time.
The audit trail is designed as a privileged, closed system:
- Userscannot stop, modify, or deletethe audit logging process.
- Audit data storage must not be directly accessible or editable by users.
Audit Trail Events
The system focuses on
business‑relevant
events, not generic technical noise.Types of Events Logged
- User Activities: Records actions performed by users during normal use of the application.
- Security and Exception Events: Captures events related to application security, including both successful and failed actions.
- Privileged Actions: Logs the use of elevated permissions or administrative capabilities.
- Authentication Activity: Tracks access to the system, including Successful and failed log‑in attempts, Log‑off events.
- Data Access Attempts: Records attempt to view or interact with data, regardless of whether the attempt was successful.
- Administrative and Configuration Changes: Captures updates made to system settings or administrative configurations.
Conceptually, each event is:
Actorperforms anActionon aTarget
- Actor: the user or system component performing the action
- Action: what was done
- Target: the resource or object affected
Audit Grid Overview
The application provides a unified, responsive audit grid that displays a consolidated view of all audit logs across
FactoryTalk DataMosaix SaaS
modules. It is designed to give users a clear, searchable, and efficient way to review system activity.Audit Trail Grid

Column Name | Description |
|---|---|
Actor | Identifies who performed the action—either an end user, system process, or machine‑to‑machine (M2M) integration. |
Event Type | Shows the category of action performed (Example, create, update, delete, login, logout, configuration change). |
Occurred Time | Records the timestamp of the event in a consistent date‑time format. |
Module Name | Indicates which FactoryTalk DataMosaix SaaS module the event belongs to (Example, Models, Extractor Configurations, Feature Flags, Auditing). |
Message | Provides contextual information about the event, such as success/failure status, key parameters, or a high‑level explanation. |
NOTE:
Actions performed in the application are captured in the audit log, but the log entries may take
up to one hour
to appear in the system.Filtering and Search
: Users can easily refine the audit log view using Date Range (From / To) filter.Sorting and Pagination
: The grid support sorting on all columns and uses server‑side pagination with a page size of 50 records.
NOTE:
The grid supports sorting, but sorting applies only to the data within the current page.
Audit Data Export
: User can export filtered audit results in CSV format
for reporting, compliance, and offline analysis, with all applied filters respected and a safe maximum record limit enforced.Provide Feedback