Change the value of a unit tag
Change the value of a unit tag using
FactoryTalk Batch
Phase Simulator.To change the value of a unit tag:
- Start theFactoryTalk Batch Phase Simulator.
- SelectEdit > Unit Tag Status.
- Make any required modifications to the Unit Tag Values, and selectUpdate Values. The new values are written into theFactoryTalk BatchPhase Simulator unit tags.
- SelectOKto return to theFactoryTalk BatchPhase Simulator window.
Provide Feedback