Unit Tag Status dialog box
Values of unit tags configured in the area model can be changed during run time in the
Unit Tag Status
dialog box.
The
Unit Tag Status
dialog box shows:Item | Definition |
|---|---|
Tagname | A list of all configured unit tags for the active area model. |
Class | The class associated with the unit tag. |
Type | The type value associated with the unit tag. |
Item | The item (addressable location) associated with the unit tag. |
Value | The current value for the unit tag. This value can be modified and sent to the
FactoryTalk Batch Server. |
Update Values | Updates the tag values in the Simulator. |
Provide Feedback