Select the filter view

The information displayed in the
e
Procedure
Client view is based upon the current filter, with the exception of the Batch List view, which displays all current batches.
To access the Filter view, click the
Select Filter
button in the Filter area of the
e
Procedure
Client page. The Filter view has two distinct areas: Equipment and Procedures.
ePro_Filter_View
The Equipment area contains the area, process cells, and units defined in your area model. Clicking one of the equipment resources returns you to the current view where the information is filtered based upon the selected resource.
The Procedure area displays all batches currently on the Batch List, including their subordinate unit procedures and operations. Phases are not listed here, as they are displayed when an operation is selected. Clicking one of the procedures returns you to the current view, where the information is filtered based on the selected procedure.
If you do not want to change the filter, click
Cancel
to return to the current view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal