Recipe secured to different network directory

Improperly secured recipes in the current working set cannot be selected when using the
Import
,
Export
, or
Generate Reports
command in the
FactoryTalk Batch Recipe Editor
. An improperly secured recipe is one in which the Security Authority Identifier (SAI) in the recipe does not match that in the current
FactoryTalk
Network Directory.
The
Improperly secured recipe
notification window opens to list any improperly secured recipes.
You can select a recipe name listed in the notification window and copy the name to the clipboard for reference.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal