Recipe impact if area model secured to different network directory
When attempting to open
FactoryTalk Batch Recipe Editor
, and a Security Authority Identifier
(SAI) mismatch exists between the area model and the FactoryTalk
Network
Directory, an error message opens.Make note of the
FactoryTalk
Network Directory and host computer information.
Then select OK
to close the error message and FactoryTalk Batch Recipe Editor
.To recover, these options are available if there is a backup of the
FactoryTalk
Network Directory SAI, or of the area model in unsecured form:- Restore theFactoryTalkNetwork Directory SAI to which the area model is secured. The name of the computer that hosts that SAI is provided in the dialog. Use theFactoryTalkAdministration Console to restore a saved backup of the SAI. TheRestorecommand is available by right-clicking on the top node in the Explorer pane. When the SAI with which the area model is associated is restored, openFactoryTalk Batch Recipe Editor.
- Open an unsecured copy of the area model inFactoryTalk Batch Equipment Editor, then select . Then, openFactoryTalk Batch Recipe Editor.
Provide Feedback