Use FactoryTalk Diagnostics Counter Monitor with FactoryTalk Linx
FactoryTalk Diagnostics Counter Monitor
aids in troubleshooting OPC connections from third-party products. It shows diagnostic information about the FactoryTalk Linx
runtime operation:- Diagnostics counters are shown as properties at AEProvider, engine, driver, protocol, data provider and shortcut levels.
- Individual diagnostic items are shown as children of their corresponding group connections.
TIP:To prevent performance degradation, run only one instance ofFactoryTalk Diagnostics Counter Monitorat a time, and close the tool when you have finished troubleshooting.
Provide Feedback