Use FactoryTalk Diagnostics Counter Monitor with FactoryTalk Live Data
FactoryTalk Diagnostics Counter Monitor
shows diagnostic information about the FactoryTalk Live Data
runtime operation:- Diagnostics counters are shown as properties at theFactoryTalk Live Dataserver andFactoryTalk Live Dataclient levels.
- Individual diagnostic items are shown as children of their corresponding group connections.
TIP:- FactoryTalk Live Datasupports diagnostics counters only under Win32 operating system, and does not support diagnostics counters in WinCE operating system.FactoryTalk Live Datadiagnostics counters only support TCP/IP protocol.
- To prevent performance degradation, run only one instance ofFactoryTalk Diagnostics Counter Monitorat a time, and close the tool when you have finished troubleshooting.
Provide Feedback