Use FactoryTalk Diagnostics Counter Monitor with FactoryTalk Alarms and Events
FactoryTalk Diagnostics Counter Monitor
shows diagnostic information about the FactoryTalk Alarms and Events
runtime operation:- Device-based diagnostics counters are shown as properties underFactoryTalk Linx/AEProviders at different levels.

- Tag-based diagnostics counters are shown as properties under Tag Alarm and Event Server at different levels.

- OPC UA diagnostics counters are shown as properties under OPC UA Alarm at different levels.

- Individual diagnostic items are shown as children of their corresponding group connections.TIP:To prevent performance degradation, run only one instance ofFactoryTalk Diagnostics Counter Monitorat a time, and close the tool when you have finished troubleshooting.
Provide Feedback