Severity
Description
Indicates the urgency of the alarm. The range of the value is from 1 through 1000. The following table describes the severity levels and the corresponding value range.
Severity level | Value range |
|---|---|
Urgent | From 751 through 1000. |
High | From 501 through 750. |
Medium | From 251 through 500. |
Low | From 1 through 250. |
Data Type
VT_UI4
Provide Feedback