Quality
Description
Indicates the quality of the data value upon which this condition is based.
Value | Definition | Description |
|---|---|---|
192 | Good | The quality is good by default. |
4 | Bad_ConfigurationError | The quality is bad because of the configuration error. |
8 | Bad_NotConnected | The quality is bad because the alarm is not connected. |
12 | Bad_DeviceFailure | The quality is bad because the device cannot be found. |
16 | Bad_SensorFailure | The quality is bad because of the sensor failure. |
24 | Bad_NoCommunication | The quality is bad because there is no communication. |
28 | Bad_OutOfService | The quality is bad because of out of service. |
Data Type
VT_UI4
Provide Feedback