Add a workstation
You may need to add a work station to
FactoryTalk Diagnostics Counter Monitor
.To add a workstation to
FactoryTalk Diagnostics Counter Monitor
:- Right-click the root in theNavigator areaand selectAdd Workstation.TheEnter Workstation IP Address/Hostnamedialog box opens.
- Enter the hostname or the device name of the target workstation, and clickOK.
Alternately, you can add a workstation by clicking the root in the
Navigator area
and:- Click
, or - From theMenubar, selectEdit > Navigator View > Add Workstation.TIP:The default workstation islocalhost.
Provide Feedback