Set Safety Network Number

  1. Choose the format for the safety network number:
    • Time-based
      . The safety network number is generated based on the creation date and time (to the millisecond) of the device. If you choose this format, select
      Generate
      to generate the number.
    • Manual
      . Enter a number from 1 through 9999, per network type. Once you have chosen your format, the safety network number appears in the
      Number
      field.
  2. Select
    Copy
    to copy your safety network number to the clipboard.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal