Device Definition view
How do I open the Device Definition view?
- On the explorer bar, select
Devices. - InDevices, double-click the controller to open the device profile.
- In the device profile, selectDevice definition.
Use
Device Definition
to:- View the device type.
- Configure device-specific settings.TIP:The parameters are based on the device being configured. The parameters that do not apply to the device are hidden.
Provide Feedback