Update controller local time dialog box parameters
Parameter | Description |
|---|---|
Set to workstation date and time settings | Sets the controller date, time, and time zone to match the
workstation settings displayed in the Workstation date
and time section. |
Manually set date and time | Configures the controller date and time manually. When
Manually set date and time is selected,
these settings display and are available to customize:
|
Adjust for Daylight Saving (+00:00) | Determines whether to adjust the controller date and time settings
for Daylight Saving. |
Provide Feedback