Date and Time view parameters
Parameter | Description |
|---|---|
Current Controller Local Time | Displays the current local time for the controller from 1/1/1970 12:00:00 AM (UTC+00:00) through 7/21/2554 11:59:59 PM (UTC+00:00),
coordinated universal time. The range varies depending on the time zone and the Adjust
for Daylight Saving (+01:00) selection. |
Adjust for Daylight Saving (+01:00) | Indicates whether the Date and Time parameter is adjusted for
Daylight Saving. The Adjust for Daylight Saving (+01:00)
parameter in this view is read-only. To change the configuration,
select Update . |
Update | Opens the Update controller local time dialog box to change
the controller local time configuration. |
Provide Feedback