Update controller local time dialog box parameters

Parameter
Description
Set to workstation date and time settings
Sets the controller date, time, and time zone to match the workstation settings displayed in the
Workstation date and time
section.
Manually set date and time
Configures the controller date and time manually. When
Manually set date and time
is selected, these settings display and are available to customize:
  • Date
  • Time
  • Timezone
Adjust for Daylight Saving (+00:00)
Determines whether to adjust the controller date and time settings for Daylight Saving.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal