Date and Time view parameters

Parameter
Description
Current Controller Local Time
Displays the current local time for the controller from 1/1/1970 12:00:00 AM (UTC+00:00) through 7/21/2554 11:59:59 PM (UTC+00:00), coordinated universal time.
The range varies depending on the time zone and the
Adjust for Daylight Saving (+01:00)
selection.
Adjust for Daylight Saving (+01:00)
Indicates whether the Date and Time parameter is adjusted for Daylight Saving.
The
Adjust for Daylight Saving (+01:00)
parameter in this view is read-only. To change the configuration, select
Update
.
Update
Opens the
Update controller local time
dialog box to change the controller local time configuration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal