High alarm high value

The alarm value entered is invalid. The
High High
alarm must be greater than or equal to
High
alarm. The
Low
alarm must be greater than or equal to the
Low Low
alarm. Check the configuration, make the required modifications, and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal