Enable HART is checked

The Enable HART check box is selected. Select this checkbox only for Input Type = Current and Input range = 4mA to 20mA.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal