Configure individual device window parameters

Configure the individual device window parameters to define the device windows.
To configure individual device window parameters
  1. On the tab for the device, expand
    Windows
    , and then select the individual device window.
  2. In the
    Window0x
    view, fill in the parameters and select
    OK
    .
    TIP:
    Use output tag member to configure parameters not editable in the
    Window0x
    view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal