Outputs view parameters

The
Outputs
view includes these parameters:
Parameter
Description
Member Name
Value
Output
The output number to which this configuration applies.
Output State During
Program Mode
Determines the value to which output changes under these conditions:
  • Device transitions to Program mode
  • Output is configured to change to Program mode when the connection is lost
C.Output0x.ProgValue
When ProgMode = 0:
0 = Off
1 = On
C.Output0x.ProgMode
0 = Go to user-defined value
1 = Hold
Output State During
Fault Mode
Determines the value to which output changes under these conditions:
  • Device transitions to Fault mode
  • Output is configured to change to Fault mode when the connection is lost
C.Output0x.FaultValue
When FaultMode = 0:
0 = Off
1 = On
C.Output0x.FaultMode
0 = Go to user-defined value
1 = Hold
Fault Mode Output State
Duration
Determines the length of time the Fault Value is held prior to the Final Fault State.
C.Output0x.FaultValueStateDuration
0 = Hold forever (default)
Any of the following:
1, 2, 5, or 10 seconds
Fault Mode Output State
Final State
Determines the value to which the output changes if these events exist:
  • Connection is lost
  • Time defined by the Fault State Duration parameter has been exceeded
C.Output0x.FaultFinalState
0 = Off
1 = On
Mode when Connection Fails in Program Mode
Determines output action if a connection faults while the device is in Program mode.
The output can remain in Program mode or transition to Fault mode.
If the output remains in Program mode, the Final Fault State is ignored.
C.Output0x.ProgramToFaultEn
0 = Remains in Program mode
1 = Transitions to the Fault mode
Enable No Load Diagnostics
Determines whether No Load detection is enabled. When No Load detection is used, if a wire is disconnected from an output that is turned off (No Load condition), the I.Outputxx.NoLoad member goes to 1.
C.Output0x.NoLoadEn
0 = Disabled (default)
1 = Enabled
Diagnostics
Opens the diagnostics dialog box to view diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal