View individual event parameters
Use the
Event0x
view to view event parameters for the input devices.To view individual event parameters
- On the tab for the device, expandEvents, and then select the extended event.
- In theEvent0xview, view the parameters for the events.TIP:To configure event parameters, navigate to theTageditor.
Provide Feedback