Device definition - Overview view
In
Device definition
, use the Overview
view to configure the device revision number, the electronic keying, and connection type for the device.
IMPORTANT:
Changing Electronic keying parameters online interrupts connections to the device and any devices that are connected through the device. Connections from other controllers can also be broken.
If an I/O connection to a device is interrupted, the result can be a loss of data.
Provide Feedback