Device definition - Counters view
In
Device definition
, use the Counters
view to define the operating mode of the counter and the Z terminal function associated with the counter. The mode of the counter determines how the A and B inputs cause a counter channel to increment or decrement. The device has two counters.
TIP:
- To configure counter parameters, setConnectioninDevice definitiontoData with EventsorData.
- The counter parameters are unavailable whenConnectioninDevice definitionis set toListen OnlyorListen Only with Events.
Provide Feedback