Counters view parameters
The
Counters
view includes these parameters:Parameter | Description |
|---|---|
Counter | Indicates the counter number to which this configuration applies. |
Rollover | Shows the rollover value. When the counter counts up to this value, it is set to the Rollunder value when the next pulse is received. |
Rollunder | Shows the rollunder value. When the counter counts down to this value, it is set to the Rollover value when the next pulse is received. |
Load Count Value | Shows the load count value. |
Load Revolution Value | Shows the load revolution value. |
Scalar | Specifies the scaling value for the counter.
|
Provide Feedback