Configure counter parameters
Configure counter parameters for the high-speed counter device.
To configure counter parameters
- On the tab for the device, selectCounters.
- In theCountersview, fill in the parameters and selectOK.TIP:Use device output tag members to configure parameters not editable in theCountersview.
Provide Feedback