Configure individual counter parameters

Configure individual counter parameters for the high-speed counter device.
To configure individual counter parameters
  1. On the tab for the device, expand
    Counters
    , and then select an individual counter.
  2. In the
    Counter0x
    view, fill in the parameters and select
    OK
    .
    TIP:
    To modify output tag member values, use the Tag editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal