Configure alarm parameters

Configure alarm parameters to alert you when the device exceeds high or low limits.
To configure alarm parameters
  1. On the tab for the device, expand
    Counters
    , and then expand an individual counter.
  2. Select
    Alarms
    .
  3. In the
    Alarms
    view, fill in the parameters and select
    OK
    .
    TIP:
    Use members to configure parameters not editable in the
    Alarms
    view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal