Outputs view parameters

The
Outputs
view includes these parameters:
Parameter
Description
Member Name
Value
Output State During
Program Mode
Determines the value to which output changes under these conditions:
  • Device transitions to Program mode
  • Output is configured to change to Program mode when the connection is lost
The
Local Control
Value is available for the devices with firmware revision 5 or later.
C.Output0x.ProgValue
When ProgMode and ProgModeLocalControl = 0:
0 = Off
1 = On
C.Output0x.ProgMode
When ProgModeLocalControl = 0:
0 = Go to user-defined value
1 = Hold
C.Output0x.ProgModeLocalControl
0 = Go to user-defined value
1 = Local Control
The
Local Control
value is available under these conditions:
  • Scan through all Windows configurations and find all counters controlling this output.
  • Verify that all counters found have been configured as Continue Counting in Program mode.
Output State During
Communication Fault Mode
Determines the value to which output changes under these conditions:
  • Device transitions to Communication Fault mode
  • Output is configured to change to Communication Fault mode when the connection is lost
C.Output0x.FaultValue
When FaultMode and FaultModeLocalControl  = 0:
0 = Off
1 = On
C.Output0x.FaultMode
When FaulModeLocalControl = 0:
0 = Go to user-defined value
1 = Hold
C.Output0x.FaultModeLocalControl
0 = Go to user-defined value
1 = Local Control
The
Local Control
value is available under these conditions:
  • Scan through all Windows configurations and find all counters controlling this output.
  • Verify that all counters found have been configured as Continue Counting in Communication Fault mode.
Communication Fault Mode Output State
Duration
Determines the length of time the
Fault Value
value is held prior to the Final Fault State.
C.Output0x.FaultValueStateDuration
0 = Hold forever (default)
Any of these values:
1, 2, 5, or 10 seconds
Communication Fault Mode Output State
Final State
Determines the value to which the output changes if these events exist:
  • Connection is lost
  • Time defined by the Fault State Duration parameter has been exceeded
Communication Fault Mode Output State Final State
is not available when
Communication Fault Mode Output State Duration
is set to
Forever
.
C.Output0x.FaultFinalState
0 = Off
1 = On
Mode when Connection Fails in Program Mode
Determines output action if a connection faults while the module is in Program mode.
The output can remain in Program mode or transition to Communication Fault mode.
If the output remains in Program mode, the
Final Fault State
is ignored.
C.Output0x.ProgramToFaultEn
0 = Remains in Program mode
1 = Transitions to the Communication Fault mode
Enable No Load Diagnostics
Determines whether No Load detection is enabled. When No Load detection is used, if a wire is disconnected from an output that is turned off (No Load condition), the
I.Outputxx.NoLoad
member goes to 1.
C.Output0x.NoLoadEn
0 = Disabled (default)
1 = Enabled
Diagnostics
Opens the diagnostics dialog box to view diagnostics information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal