Diagnose a problem with a point
Diagnose these point problems from the
Outputs
view:- Whether a fault exists.This fault indicates that a fault is present on the device.
- Whether a short circuit fault exists.This fault indicates that a short circuit or over current condition exists.
- Whether a no load fault exists.This fault indicates that the signal wire is disconnected from the output or the RTB is removed from the device.
To diagnose a problem with a point
- On the tab for the device, selectOutputs.
- In theOutputsview, in theDiagnosticscolumn for the point, select
. - InOutput0x Diagnostics, view the diagnostics for the point.
Provide Feedback