Device definition - Overview view parameters
The
Overview
view in Device definition
includes these parameters:Parameter | Description |
|---|---|
Device type | Displays the device catalog number and type. |
Name | Enter an IEC 61131 compliant device name. If an invalid character is entered in this field, or if the name exceeds 40 characters, the software ignores the character. |
Description | Enter the description of the device. The description must be within 512 characters. If the description exceeds the maximum length, the software ignores any extra characters. |
Slot | Specifies the slot number where the device resides. |
Series | Specifies the series of the device. |
Revision | Specifies the major and minor firmware revisions of the device. |
Electronic keying | Reduces the possibility of using the wrong device in a control system. Available options are:
IMPORTANT:
|
Connection | Determines these items for the device type you configure:
Connection affects the configuration options available in Device definition and determines what data is exchanged between the owner-controller and the device. |
Provide Feedback