Search
5069 SERIAL
Troubleshooting
Invalid value
Invalid character
Invalid character value
Invalid data format combination
Invalid pad character value
Invalid receive delimiter value
Invalid start delimiter value
Invalid termination delimiter values
Invalid termination delimiter 1 value
Invalid termination delimiter 2 value
Response Timer must be greater than Inter-Frame Timeout
Value is over range
Value is under range
Modbus data size is exceeded
Register start address values are overlapping
Data index values are overlapping
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal