Channel X view

Use the
Channel
X
view to configure the serial protocol for the channel.
Use the
Channel
X
view to:
  • Set the
    Baud Rate
    ,
    Data Bits
    ,
    Parity
    , and
    Stop Bits
    .
  • Select whether the serial media is
    RS-232C
    ,
    RS-422
    , or
    RS-485
    .
  • Select the
    Duplex
    for the serial media.
  • Specify the delay between the time the RTS signal changes from low to high and the time data is sent.
  • Specify the delay between the time the last character is sent and the time the RTS signal changes from high to low.
  • Specify the Data Carrier Detect (DCD) wait delay time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal