Channel X - Generic ASCII Transmit view
Use the
Channel
view to define the data transmitted to the serial device.X
- Generic ASCII TransmitUse the
Channel
view to:X
- Generic ASCII Transmit- Select the swapping mode for data transmitted to the serial port.
- Select the termination mode.
- Specify the termination delimiters.
- Open the diagnostic dialog box to diagnose a communication problem with the Generic ASCII Receive/Transmit communication.
The
Channel
view is available when X
- Generic ASCII TransmitChannel
in X
Device definition
is set to Generic ASCII
.Provide Feedback