SSI – Input for Store Function view parameters

The
SSI – Input for Store Function
view includes these parameters:
TIP:
This view is only available when you use Input00 as a trigger for the "Store" counter function.
Parameter
Description
Input00
Off → On
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input00
On → Off
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal