Module Tag definitions
The tags that are available vary depending on module type and selections that are made in
the
Device Definition
.The types of module tags include:
- Configuration (as indicated by a "C")
- Input (as indicated by an "I")
- Output (as indicated by an "O")
- Event Input (as indicated by an "EI")
- Event Output (as indicated by an "EO")
Provide Feedback