Device Definition – Counter view parameters
The
Counter
view in the Device Definition dialog includes these parameters:
Parameter | Description |
|---|---|
Mode | Specifies the mode in which the counter operates. Available options are:
|
Invert Input A | Specifies whether to invert the indicated input.
This parameter is only available when the counter mode is
configured as Count/External Direction, Count/Internal
Direction, or Up/Down Pulses. |
Invert Input B | Specifies whether to invert the indicated input.
This parameter is only available when the counter mode is
configured as Count/External Direction, Count/Internal
Direction, or Up/Down Pulses. |
Invert Input A, B | Specifies whether to invert the indicated input.
This parameter is only available when the counter mode is
configured as Quadrature X1, Quadrature X2, or Quadrature
X4. |
Input Z Function | Defines the function for the indicated input.
Each counter function (Reset, Store, Load, Hold) can only be
triggered by one input. For example, if you select the Input Z Function as "Reset, Hold",
then the options that contain "Reset" and "Hold" are not
available to select for the Input00 Function. If you select any option for Input Z Function, then Input00
Function is automatically set to Not Used. |
Invert Input Z | Specifies whether to invert the indicated input.
|
Input00 Function | Defines the function for the indicated input.
Each counter function (Reset, Store, Load, Hold) can only be
triggered by one input. For example, if you select the Input Z Function as "Reset, Hold",
then the options that contain "Reset" and "Hold" are not
available to select for the Input00 Function. If you select any option for Input Z Function, then Input00
Function is automatically set to Not Used. |
Invert Input00 | Specifies whether to invert the indicated input.
|
Provide Feedback