Test Output Ptxx Diagnostics view parameters (5034-IB8S)
The
Test Output Ptxx Diagnostics
view for the test outputs includes these
parameters:
Parameter | Description |
|---|---|
Fault Exists | Displays whether a fault is present. |
Field Power | Displays whether field power is present on the point. |
Field Power On Timestamp | Displays the timestamp of the last time field power turned on
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Field Power Off Timestamp | Displays the timestamp of the last time field power turned
off in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Short Circuit Fault | Displays whether a short circuit (short to high) fault is
present on the point. |
Short Circuit Fault Timestamp | Displays the timestamp of the last short circuit fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Overload Fault | Displays whether an overload fault is present on the
point. |
Overload Fault Timestamp | Displays the timestamp of the last overload fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Internal Fault | Displays whether an internal fault is present on the
point. |
Internal Fault Timestamp | Displays the timestamp of the last internal fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
No Load Fault | Displays whether a No Load fault is present on the point. |
No Load Fault Timestamp | Displays the timestamp of the last No Load fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Provide Feedback