Ptxx Diagnostics view parameters (5034-OB8S)

The
Ptxx Diagnostics
view for the outputs includes these parameters:
Parameter
Description
Fault Exists
Displays whether a fault is present.
Data Uncertain
Displays whether the module is operating outside the designed operating range.
Field Power
Displays whether field power is present on the point.
Field Power On Timestamp
Displays the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Field Power Off Timestamp
Displays the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Short Circuit Fault
Displays whether a short circuit (short to high) fault is present on the point.
Short Circuit Fault Timestamp
Displays the timestamp of the last short circuit fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Overload Fault
Displays whether an overload fault is present on the point.
Overload Fault Timestamp
Displays the timestamp of the last overload fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Internal Fault
Displays whether an internal fault is present on the point.
Internal Fault Timestamp
Displays the timestamp of the last internal fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Dual Channel Fault
Displays whether a dual channel fault is present on the point.
Dual Channel Fault Timestamp
Displays the timestamp of the last dual channel fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
No Load Fault
Displays whether a No Load fault is present on the point.
No Load Fault Timestamp
Displays the timestamp of the last No Load fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Over Temperature Fault
Displays whether an over temperature fault is present on the point.
Over Temperature Fault Timestamp
Displays the timestamp of the last over temperature fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Critical Temperature Fault
Displays whether a critical temperature fault is present on the point.
Critical Temperature Fault Timestamp
Displays the timestamp of the last critical temperature fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal